Aktuelles und Veranstaltungen

 
   

CUI Acquires Tectrol

TUALATIN, Oregon, 2. März 2015 - CUI Inc und seine Muttergesellschaft CUI Global Inc. (NASDAQ:CUI), have announced that they have entered into a definitive agreement under which CUI will acquire specific assets of the privately held Canadian equipment manufacturer Tectrol, Inc, a leading designer and manufacturer of standard and custom power solutions.



▸ Read Press Release

 

Mouser Electronics Signs Global Distribution Agreement with CUI

Mouser Electronics, der weltmarktführende Vertragsdistributor mit den neuesten Halbleiter- und Elektronikbauelementen, hat heute den Abschluss eines weltweit geltenden Vertriebs- und Partnerschaftsabkommens mit CUI Inc bekannt gegeben, seit über 25 Jahren einer der Weltmarktführer in der Entwicklung und im Vertrieb von elektromechanischen Bauelementen.

▸ Read Press Release

 

Join us at APEC 2015

At the upcoming Applied Power Electronics Conference (APEC) 2015, CUI will be demonstrating the latest product releases from the company's award winning Novum® Advanced Power product line. CUI's booth will also showcase a fully digital power system featuring modules from each member of the newly formed Architects of Modern Power (AMP Group) consortium.

Visit CUI at booth 206

▸ Visit Event Page

 
 

New Products

Ressourcen

Die CUI Produktlinie externer Stromversorgungen wurde erweitert, um Stufe-VI-Effizienzstandards zu erfüllen

The SWI12-SC and SWI24-SC Series feature screw terminal connections for designs that require flexibility beyond the standard 5 foot dc cord, including security, home automation and smart applications. The 12 W and 24 W adapters also meet Level VI efficiency standards set to go into effect in 2016, keeping our customers one step ahead of the more stringent US regulations.

  • Up to 24 W continuous power
  • Level-VI-Effizienz
  • Universeller Eingangsspannungsbereich
  • Schraubklemmen
  • No load power consumption < 0.1 W
  • Überströme-, Überspannungs- und Schaltkreisschutz
  • UL 60950 & UL 1310 safety approvals

SWI12-SC Series / SWI24-SC Series

Application Note

The global regulatory environment surrounding the legislation of external power supply efficiency and no-load power draw has rapidly evolved over the past decade. With the publication of a new set of requirements by the United States Department of Energy (DOE) set to go into effect February 2016, the landscape is set to change again.

Read App Note


Editorial Article

In the January 2015 EDN Power Forward blog post, CUI Senior Vice President, Mark Adams, discusses the significance of the Internet of Things (IoT) and its overall impact on energy efficiency and power consumption.

Read on EDN

Contest

Open-Frame-AC/DC-Netzteile

CUI's next-generation VOF open frame ac-dc power supply series delivers higher efficiency and improved no-load performance to meet the growing demand for green power technology. Der VOF weist Branchenstandard-Abmessungen auf. Durch das effiziente Design, die kompakte Größe und absolute Zuverlässigkeit sind diese Stromversorgungen die ideale Lösung für eine Vielzahl von Verbraucher-, Industrie- und ITE-Anwendungen.

Question: CUI's open frame ac-dc power supplies have efficiencies up to what percentage?

Submit your answer to contest@cui.com

(Five winners will be selected on 30.3.2015. Winners will be notified via email.)

20050 SW 112th Avenue
Tualatin, OR 97062 USA
+1 800 275 4899
www.cui.com

          

 

Powered By OneLink