CUI auf Shortlist für zwei 2015 ECN Impact Auszeichnungen

5.5.2015


CUI auf Shortlist für zwei 2015 ECN Impact Auszeichnungen

CUI Inc and its industry leading products have been announced as finalists in two separate categories for the 2015 ECN Impact Awards. Der Wettbewerb zielt darauf ab, die weltweit besten und innovativsten Unternehmen der Konstruktionstechnik zu ehren.

CUI’s rugged, high accuracy AMT31 commutation encoder series was named as a finalist for the Electromechanical/Mechanical Devices category, which honors the continuous innovation of components that move or have moving parts, including electromechanical switches, motors, servos and more. CUI’s NDM3ZS-60 series was also named a finalist in the Power Sources and Conditioning Devices category recognizing devices used to supply and/or manipulate power. The 60 A Novum® digital POL dc-dc converter module is a part of a wide open product category that understands that power is the backbone of the electronics industry, with limitless potential applications.

The winners in each award category will be announced at the second annual ECN Impact Awards ceremony at the Mirage, Las Vegas on 13. Mai 2015 in conjunction with EDS 2015, a premier electronics distribution event put on by the Electronic Components Industry Association (ECIA) and Electronics Representative Association International (ERA).

Additional information about the 2015 ECN Impact Awards can be found here.

Weitere Details zur AMT31-Serie

Weitere Details zur NDM3ZS-60-Serie





 
Powered By OneLink