Lösen der Herausforderungen in Sachen Stromkapazität mit Software Defined Power®

26.9.2016


Lösen der Herausforderungen in Sachen Stromkapazität mit Software Defined Power®

In the September 2016 edition of Bodo’s Power Systems, CUI’s Senior Vice President, Mark Adams, discusses power capacity challenges in datacenter infrastructures and how CUI’s partnership with Virtual Power Systems (VPS) is taking a hardware and software approach to solve those inefficiencies. Included with the article is a full-page front cover designed by CUI’s Marketing team.

The article begins, “Running out of power is a constant concern for the operators of data centers and similar IT and communications infrastructure. Das Ringen um Unterbauoptimierung bei gleichzeitiger Steigerung der Processing- und Speicherkapazität ist ein nie endender Kampf. However, the inefficiencies and underutilization of current power supply infrastructures that are designed to meet peak demand can now be avoided using a combination of hardware and software to even out supply loading and optimize the available capacity.”

 Read the full Bodo's article

Learn more about Software Defined Power®



 
Powered By OneLink