Lastschaltung: Was sind die nächsten Wachstumsbereiche für digitale Stromversorgungen?

28.6.2013


Lastschaltung: Was sind die nächsten Wachstumsbereiche für digitale Stromversorgungen?

CUI’s latest Power Forward blog post addresses the question “What are the next growth areas for digital power?” In dem Artikel verweist Mark Adams auf den vor kurzem aktualisierten IHS Bericht zur digitalen Stromversorgung und verweist auf ein laufendes Missverständnis innerhalb der Branche.

The post begins, “It's widely acknowledged that digital power has been almost exclusively used by OEMs developing IT and communications infrastructure - indeed, servers are the largest single market for digital power, accounting for an expected 33 percent of market revenue in 2013.

Because growth has historically originated from this one sector, digital power device manufacturers have catered their technology and design infrastructure specifically to this market, at the expense of mass market adoption.

“Digital power benefits virtually all applications, but it hasn’t been clear when it would make the move from a niche technology to the mass market…”

Read the full article on edn.com
Learn more about CUI’s Novum® Advanced Power line



 
Powered By OneLink