Paultre on Power - Mark Adams of CUI at APEC 2015 (Podcast)

30.3.2015


Paultre on Power - Mark Adams of CUI at APEC 2015 (Podcast)

In this podcast Mark Adams, CUI's Senior VP, talks to Alix Paultre of Power Systems Design about the latest digital power solutions from CUI's Novum® Advanced Power line at the 2015 Applied Power Electronics Conference (APEC).

From the Power Systems Design website:

"CUI released its highest-current digital POL family to date at the event. Designed specifically to address the rapidly-rising power requirements of today’s most advanced integrated circuits, the NDM3Z-90 is a non-isolated module outputting 90A in ultra low-profile vertical and horizontal packages. The series delivers benchmark power levels while incorporating a range of advanced digital features."

Listen to the podcast on powersystemsdesign.com

Weitere Informationen über CUIs Novum Advanced Power Produktlinie



 
Powered By OneLink