CUI Inc’s NSM2P Series Wins Product of the Year Award from Electronic Products Magazine

8.1.2013


CUI Inc’s NSM2P Series Wins Product of the Year Award from Electronic Products Magazine

CUI Inc announced that Electronic Products Magazine, a key publication for important developments in products and product technology within the electronics industry, has named the NSM2P “No-Bus” digital point-of-load (POL) series as a Product of the Year for 2012. Aus Tausenden von Produkten wählten die Redakteure von Electronic Products die siegreichen Beiträge auf der Grundlage eines bedeutenden Fortschritts der Technologie oder ihrer Anwendung, einer Designinnovation oder eines Preis/Leistungsgewinns aus.

The NSM2P series is a unique iteration of CUI’s class-leading Novum® Advanced Power digital POL modules. The No-Bus series is designed specifically for customers who value the performance advantages inherent in digital power but do not want to incorporate digital bus communication in their systems. The modules allow customers to access a full suite of digital parameters during the development stage where the desired functions can be tested and manipulated within the system through CUI's simple to use graphical user interface (GUI). The NSM2P series offers the flexibility of digital power in a device that is simple to integrate within a power system.

“We are honored to have received this award from Electronics Products Magazine,” said Matt McKenzie, President of CUI Inc. “2012 was a game-changing year for our Novum® Advanced Power Division and it is a privilege for CUI and its Design Team to be recognized among the top companies who have produced the electronic industry’s most innovative, successful products and services.”

“The editors of Electronic Products Magazine awarded the prestigious Product of the Year to CUI for its NSM2P because it was the first self-compensating point-of-load dc/dc module that doesn’t need a digital bus,” said Senior Editor Paul O’Shea. “Hence designers don’t need to learn digital commands as it allows the engineers to set limits for voltage, current, and temperature by developing a configuration file via a graphical user interface. This makes it easy for developers to change and even store additional configurations for simple access, and with no hardware changes.”

Additional information about the NSM2P Product of the Year Award can be found online at http://www2.electronicproducts.com/CUI_Digital_PoL_modules_need_no_digital_bus-article-poypo01_CUI_NSM2P_JAN2013-html.aspx.



Weitere Nachrichten




 
Powered By OneLink